LDO精准电源是内部提供的,但输出不是1.8V,测得输出1.92V,这也差距太大了吧?实在不知道是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
这个是正常的,片内LDO精度不是很高,一般在±10%,在这个范围内都是符合要求的。
我的模拟输入电压是5V时候,数据端却得不到0X7FFFFF,按照数据手册的话,是不是应该输入最大的时候得到这个值,但却只能达0X6bxxxx(x代表任意值)。
Pcm1865Evm也是用的内部的LDO,那它的输出正确不?
Pcm1865Evm也是用的内部的LDO,那它的输出还正确不?
那模拟输入端满量程的时候,输出端的数据是满量程吗?
Hi,
是的,I2S的数据输出格式是2的补码表示,输入信号(单端或差分)达到2.1Vrms时,I2S的数据就满量程了。