This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6120A2

Other Parts Discussed in Thread: TPA6120A2

老师,请问TPA6120A2的输出匹配电阻是否可以减小,因为现在的耳放都要求阻抗要小,我原来设计使用的是10欧,现在想减小为2.2欧或更小,是否可行?减小了会存在什么风险?

  • 您是指的输出端串行的电阻值吗?那个电阻建议是10ohm~100ohm。

  • 如果指的串行输出电阻值的大小,不建议低于10ohm连接,datasheet中其实也有描述:The series output resistor should be between 10Ω and 100Ω. The output series resistance eases the work of the output power stage by increasing the load when low impedance headphones are connected, as well as isolating any capacitance on the following traces and headphone cable.

    这里的隔离电容,指的是PCB trace 带来的寄生电容的影响,这里的串联电阻起到了隔离电容的作用,因为我们知道运放带容性负载的话会非常不稳定,所以这里的串联电容也起到了一个隔离保护的作用。