Other Parts Discussed in Thread: TAS5711, TAS5731, TAS5731M
1. 客户在使用TAS5711时,工作时功能都正常,但是在无音频输入时,IC温度会到62度左右,手摸会有点点温度的感觉,而TAS5731 同样条件测试则温度在55度,但在正常工作时,温度在80度以内,是正常范围内。请问在无音频信号输入时,这个62度的温度是正常的吗?EVM板上是没这么高温度的,客户的板子是2层板条件。
2. 在使用TAS5731M时,开始播放音乐功能正常,在做扫频测试时,发现档频率扫到18K 以上时,IC会无输出,检测0x02寄存器没有发现异常,重新上电后还是无输出。请问有可能是什么原因会造成这种现象 ?OC pin 是上件22K,有没有可能是这个值的原因造成的 ?