Other Parts Discussed in Thread: TPA6133A2
最近的一个项目做便携产品要用到耳放 挑选TPA6133A2这个芯片 确认下该芯片的19脚SD电平动作
上电工作有音乐的时候19脚SD电平是高电平不?
静音不放音乐的时候19脚SD电平是低电平不?
还请工程帮忙确认下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPA6133A2
最近的一个项目做便携产品要用到耳放 挑选TPA6133A2这个芯片 确认下该芯片的19脚SD电平动作
上电工作有音乐的时候19脚SD电平是高电平不?
静音不放音乐的时候19脚SD电平是低电平不?
还请工程帮忙确认下,谢谢
SD低有效,指的是TPA6133A2低功耗模式,当TPA6133A2正常工作时为高电平,低功耗模式为低电平。
如果TPA6133A2不是低功耗模式,SD就一直为高。
或者说在上电过程中,SD是一个由低到高的变化过程。VCC从0V到VCC电压稳定之后,SD变高。
我现在产品的SD电平动作是这样的,上电开机SD先瞬间1.4V 立马转为0V
正常有声音的时候SD为1.4V
6133A2的输入4个电容改变大小音质改变大不?