Other Parts Discussed in Thread: TL971, OPA1641
Hi TI team,
之前是采用TL971,由于971驱动能力相对较弱,所以换成了P2P兼容的OPA1641。要求是OPA1641可以有4V的峰峰值输出,音频运放的输出信号通过电容C76耦合到TPS76301的输入端。下面是原理图。
问题:运放与LDO连接,当断开电容C76后发现功放输出只有1V,请教一下这是什么原因呢,多谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不断开C76输出正常? TL971和OPA1641情况都相同?
另外,输出串联C76的作用是什么?
Hi Kailyn,
Sorry, 我说错了。
C76的作用是将运放输出的交流信号叠加到外部输入的直流8V上。
现在问题是:若LDO和运放断开单独测试,运放输出信号正常,但是如果和外部8V叠加后连接到LDO输入端,测试发现运放输出脚信号会严重失真。
问下您是否有什么建议呢?谢谢