Other Parts Discussed in Thread: OPA1611, MAX660, TPS65133, INA137
我的设备使用了OPA1611音频运放对CODEC输出的单端音频信号进行放大后送到话机扬声器(要求单端音频),音频运放使用单端5V电源进行供电,放大倍数为5,此5V电源同时给MCU供电,。当我在触摸屏上滑动手指或者点击屏幕上图标时,可以从话机扬声器听到“哒哒”声,将CODEC与OPA1611之间断开后仍存在“哒哒”声;示波器测量发现触屏时5V电源有波动。请问如何消除该“哒哒”声,以下哪个方案是否可行,有没有更好的方法
1.使用MAX660做反压器,使用+5V、-5V给OPA1611供电;
2.使用TPS65133将3.3V升压到+5V、-5V给OPA1611供电;
3.CODEC输出差分音频,进行差分放大,再使用INA137进行差分转单端,提供给话机扬声器;
谢谢。