Other Parts Discussed in Thread: PCM4220, LMK00105, PCM4222, TAS5558
新年好!由于本人学识有限 求解答!我想用下面这个晶振和LMK00105时钟缓冲器,给pcm4220提供时钟源,可是器件之间的时钟信号输入输出阻抗不知道怎么设计?HCMOS与LVCMOS晶振的输出内阻是一样的吗?pcm4220的MCKI时钟输入阻抗不知道哦!求给个设计法!谢谢
了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
12.288MHz的有源晶振吗?可以直接给PCM4222提供时钟。您的本意是想加一个时钟缓冲再给PCM4222?
PCM4222 EVM板上采用的24.566MHz的有源晶振,然后通过D类触发器,实现频率2分频之后给PCM4222。
你好!12.288M的晶振不只是给pcm4220提供时钟,同时还要给1个tas5558提供12.288的时钟。我的第一块实验板暂时只有1个tas5558,最终我会用2个12.288M的有源晶振,一个直接给pcm4220、另一个是经过lmk00105给5个tas5558提供时钟。
lmk00105数据手册中说; as shown as below. If driving a transmission line with higher characteristic
impedance than 50 ohms, a series resistor (Rs) should be placed near the driver to provide source termination,
where Rs = Zo – Ro,如果我用12.288M,HCMOS输出的有源晶振,需要怎么来匹配Rs的阻值。所有的有源晶振都没有提供Ro的值就没法计算啊!只提供了输出负载电容15pF的值。公式中的Zo是不是固定的值50 ohms?