大家好,我现在使用TLV320AIC34实现4路单声道音频输出,很多设计是将立体音输出,这样会占用两个DAC,达不到4路音频输出的效果,如果一路DAC对应一路单声道音频,请问原理图应该如何设计?是不是应该HPLOUT_A、HPLOUT_B、HPROUT_A、HPROUT_B分别接一个座子?其他的HPLCOM_A等悬空?
我的音频座子是立体音的, 是不是需要将HPLOUT_A分别接座子上的L和R?
望知情者告知,感激不尽。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我现在使用TLV320AIC34实现4路单声道音频输出,很多设计是将立体音输出,这样会占用两个DAC,达不到4路音频输出的效果,如果一路DAC对应一路单声道音频,请问原理图应该如何设计?是不是应该HPLOUT_A、HPLOUT_B、HPROUT_A、HPROUT_B分别接一个座子?其他的HPLCOM_A等悬空?
我的音频座子是立体音的, 是不是需要将HPLOUT_A分别接座子上的L和R?
望知情者告知,感激不尽。
Hi Yang,
你好!
根据你的描述,你想用TLV320AIC3106实现4路单通道音频输出。请你输入准备如何配置,4路单声道音频信号都是从模拟输入还是会有从数字的Audio serial bus interface 输入?还有就是4路信号是不是需要完全独立?输出负载大概多少,准备出多少功率?
如果你是全模拟输入,因为TLV320AIC3106内部的两路ADC和DAC都是Stereo的,其输出也是stereo,他们无法直接拆开为独立的mono的两路。但是根据从系统功能框图可以看出来,LINE2LP/M和LINE2RP/M可以通过寄存器配置直接输出,配合stereo的两路ADC+DAC可以凑成4路。具体请参考Datasheet 的P31 11.3.4 到11.3.6小节和application部分。
Regards,
Alix Wan