This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1864 PDM 输入 增益问题

Other Parts Discussed in Thread: PCM1864

请问PCM1864 从PDM输入讯源 到I2s输出 测量发现 有增益7.1dB?

测量方法 从Apx555 分析仪 送PDM讯源 到PCM1864 PDM透过 I2S输出测量输出 发现有7.1db增益 ,

以确认相关暂存器PGA预设值都是在0db

不清楚这7.1db增益 怎产生 ,这是正确的吗

谢谢

  • PDM输入,那么您应用使用的是digital PGA, analog PGA需要bypass掉,通过0X19进行寄存器的配置。
    另外,7.1dB这个数值是不正确的,digital PGA的增益间隔是0.5dB。 而增益的配置要看下0X19您是手动配置,还是自动配置增益的?
  • 你好 确认过0x19 预设值 00 自动配置 测过 , 也改过手动配置x19=FF 设定DPGA _VAL 0x16= 设定0db 测试结果 还是有增益7.1db
    analog PGA bypass是哪个暂存器 ,有关闭ADC input 這樣算bypass 嗎 謝謝