This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tlv320aic3101的Output common-mode 电压大小指的什么?



Output common-mode 电压的默认值是1.35v ,在AVDD_DAC = DRVDD = IOVDD = 3.3 V, DVDD = 1.8 V, fS = 48 kHz, 16-bit audio data, HPLOUT设置为单端模式 条件下,改变这个值的设定会影响到模拟输出电压的RMS值吗?

  • 您好,

    如果是差分输出,Output common-mode则 是同向输出端电压V+与反向输出端电压V-之和除以2,即(V+ + V-)/2。
    单独输出,Output common-mode则 是输出电压与参考点电压之和除以2。

    RMS值是输出信号不失真的情况下输出信号的有效值,输出不失真情况下峰峰值为 √2*VRMS,如果改变输出共模电压,可以输出的峰峰没有变,但是如果输出同样的信号,实际输出的信号会失真。