Other Parts Discussed in Thread: TPA3251, TPS3802
当把TPA3251的FAULT接到TPS3802 MR脚后 ,RESET输出一直为低电平,导致TPA3251无法启动。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
建议做以下测试(因为reset信号和fault信号都与TPA3251 芯片有关,排除自锁这种情况):
1、断开TPS3802 输出至TPA3251 的Reset信号,给TPA3251 reset管脚一个高电平看下TPA3251 是不是正常工作的?
有可能是TPA3251 没有正常工作,导致FAULT输出低电平,进而使TPS3802的reset输出低电平,而在TPA3251 复位时,fault管脚又输出高电平。
2、断开TPS3802 输出至TPA3251 的Reset信号,即将TPS3802 reset 管脚输出悬空,测试TPS3802 reset 管脚电平状态。
1.拆掉TPA3251后,只保留时TPS3802时,RESET能够输出高电平。测量VDD脚有3.3V,MR脚有3.18V,RESET脚有3.3V。
2.拆掉TPS3802后,给TPA3251的RESET脚高电平(MCU模拟),同时测量FAULR脚有高电平,TPA3251能够正常启动并有声音出输。
3.TPS3802,TPA3251保留时,只是断开FAULT与MR之间的链接(0Ω电阻),TPA3251能够正常启动并有声音输出。测量TPS3802的VDD脚有3.3V,MR脚有3.18V,RESET脚有3.3V。测量TPA3251的RESET脚有3.3V,FAULT脚有3.3V。
以下是疑问点:
4.TPS3802或者TPA3251,当独立时都可能正常工作。但是只要把FAULR与MR连通后,TPS3802的RESER脚就没有输出高电平了。