This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tpa3221



Dear All

        

芯片的第22脚GVDD,规格书要求为串联3.3R电阻,电压为4.5-5.5V;

      但我们现在串联的是1K电阻,电压为4.2V,经测试这个4.2V是稳定的,无论小功率还是大功率输出都对这个电压没有影响;并且我将电阻改为51K,电压依然为稳定的4.2V,测试所有功能依旧正常!

      那么,问一下,这个电压为4.2V时,对于芯片工作有什么影响?我们现在电压为4.2V,芯片工作会有什么隐患?

 

  • 您好,

    GVDD电压是为门极驱动电路供电的,范围4.5V到5.5V,MOS导通电压有一致性问题,GVDD电压最低4.5V保证所有芯片中MOS能够正常导通,数据手册中各参数也是在GVDD=5V给出的,电压为4.2V不能保证数据手册中的电气特性。