TI工程师,PCM2707C的EVM电路图中,有个存储器,这个IC里面需要存储什么信息?如果没有这个存储器可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用PCM2707C输出S/PDIF信号,然后后端接DIR9001,PCM2707C输出没有经过其它电路,因为在DIR9001的输入已经有了。现在实际使用发现,当我在电脑上设置输出采样率44.1K的时候,DIR9001经常发生锁频错误,大约3-5分钟一次。如果设置为48K的时候,DIR9001的锁频错误提示更频繁,大约20-30秒会出现一次。使用其他的S/PDIF信号的时候,DIR9001没有发生类似问题。基本可以确定是PCM2707C出现的问题,在设置输出I2S的时候,也会发生。这种情况,应该如何分析,如何排查问题呢?
测量信号非常正常,开始因为DIR9001的接入端的75R电阻导致波形有点失真,可能负载比较大,我把后端的电阻去掉以后,波形非常好。VO H和VO L都能够正常上下变化,对比其他的USB转I2S芯片,都输出44.1的采样率,波形的时序基本是一样的,只是另外一块板子波形毛刺很多,存在很大的过冲现象。
我现在是导入的文件,你看看能不能看到。