Part Number: TAS2521
你好,想请教以下几个问题
1.在播放音乐的时候,只要将音量调到最大,喇叭就会自动mute。这种情况的是不是输出功率过大导致的过流保护?
2.为什么在播放单频或者粉噪声的时候,就算播放0dB的音频也没有出现喇叭会自动mute的现象,这是为什么呢?
3.在TAS2521的datasheet中有提及过流保护,但是没有说该怎么控制,想请问一下关于过流保护是否可以关闭?关闭之后会不会存在其他问题?该怎么关闭可否提供寄存器地址呢?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS2521
你好,想请教以下几个问题
1.在播放音乐的时候,只要将音量调到最大,喇叭就会自动mute。这种情况的是不是输出功率过大导致的过流保护?
2.为什么在播放单频或者粉噪声的时候,就算播放0dB的音频也没有出现喇叭会自动mute的现象,这是为什么呢?
3.在TAS2521的datasheet中有提及过流保护,但是没有说该怎么控制,想请问一下关于过流保护是否可以关闭?关闭之后会不会存在其他问题?该怎么关闭可否提供寄存器地址呢?

您好,
1、TAS2521没有输出可能由2种原因造成,1个是您指出的过流保护,另1个是您截图下方所示的过热保护OTP;您可以通过读取寄存器P0_R46_D7和P0_R45_D7来判断是否发生了过流或过热保护。
2、这里您想说明什么问题?
3、查看您附的截图第三段:The TAS2521 has a short-circuit protection feature for the speaker drivers that is always enabled to provide protection.因此是无法关闭过流保护的
非常抱歉,回复晚了,不知道您的问题解决了没有?
您是输入的数字音频信号,还是模拟音频信号?关于下面引用的现象,您多换几个音频源看看是不是有同样的现象?
播放音乐的时候会出现没有输出的现象,但是我在播放单频或者粉噪声(都是0db的信号,这个信号已经是最大的),都没有出现没有输出的现象
The TAS2521 has a short-circuit protection feature for the speaker drivers that is always enabled to provide protection. If the output is shorted, the output stage shuts down on the overcurrent condition. (Current limiting is not an available option for the higher-current speaker driver output stage.)这句话的意思是如果输出端短路,输出级就会 shuts down,SPK 驱动输出级没有电流限制功能,满足过流条件就直接关断(shuts down)