Other Parts Discussed in Thread: TAS5760LD,
TAS5760LD可以替代TAS5760MD吗?它们的主要差异是什么?规格书上没有明显注明。开发新产品需选择型号,希望帮忙指导一下?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好, 在TAS5760MD的datasheet中有给出比较的表格,主要区别在于TAS5760MD不支持3 wire I2S mode 而尾缀为LD的几款除了TAS5760LDDCA都支持3 wire I2S 模式。
Hi Kailyn,谢谢您的回复!
目前我们产品现状使用的是TAS5760MDDCA,因为此料没有库存了,希望使用TAS5760LDDCA替代,可以实现吗?
如可以的话,希望麻烦您帮忙告诉一下我们的外围电路或软件需要如何修改吗?
您好,参考上面表格比较,TAS5760MDDCA和TAS5760LDDCA的主要区别在于PVDD的电压范围不一样,TAS5760LD的PVDD电压范围为4.5V~16.5V,TAS5760MD的PVDD范围为4.5V~26.4V电压 ,并且我看了下二者的内部架构以及寄存器信息都是一样的,所以如果PVDD的电压也满足您的应用之外,我认为是可以替换的。
您好,是的,同样PVDD电压的条件下(16.5V以内) 是不会影响输出功率的,但是因为TAS5760MD的PVDD电压能达到26.4V, 那么同样负载的条件下肯定,能得到更大功率的输出,Pout=(Vrms)^2/R,。