Part Number: TAS5760M-Q1
您好
我在使用TAS5760,输入信号和电源无问题,但是无输出, AVDD电压12V,有以下疑问
1.SPK_SD(pin #7)always high,这样是否可以?
2.要使内部的DVDD LDO输出电压,除了给到AVDD电压并pull-high SPK_SD,还依赖其他什么信号吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS5760M-Q1
您好
我在使用TAS5760,输入信号和电源无问题,但是无输出, AVDD电压12V,有以下疑问
1.SPK_SD(pin #7)always high,这样是否可以?
2.要使内部的DVDD LDO输出电压,除了给到AVDD电压并pull-high SPK_SD,还依赖其他什么信号吗?
您好,上电过程SPK_SD 是一个由低到高的变化过程。 不建议一上电就直接上拉,当电压起来稳定,clock信号稳定之后再将此引脚拉高。
2.不需要,电压起来稳定之后,TAS5760进入正常,内部LDO的输出引脚ANA_REG会有电压输出。
另外,没有输出,读取下寄存器0x01的bit1 SPK_SLEEP是否=1,使得TAS5760进入sleep状态。
hi Kallyn
多谢你的建议;答复如下:
1.上电过程SPK_SD 是一个由低到高的变化过程。 不建议一上电就直接上拉,当电压起来稳定,clock信号稳定之后再将此引脚拉高。
→我断开SPK_SD脚并用飞线引出(线路上有下拉电阻),等AVDD上电后将SPK_SD飞线到板上其他的3.3V电源。
2.不需要,电压起来稳定之后,TAS5760进入正常,内部LDO的输出引脚ANA_REG会有电压输出。
→按如上这样操作,ANA_REG pin并没有电压输出
3.另外,没有输出,读取下寄存器0x01的bit1 SPK_SLEEP是否=1,使得TAS5760进入sleep状态。
→我们就是期望使用TAS5760内部的LDO产生3.3V,现在ANA_REG没有电压输出,所以DVDD没电,无法用I2C读取寄存器。如果用板上其他3.3V驱动DVDD,则违背我们设计初衷。
您好,电路没什么问题,但是关于您提到的第三条,DVDD没电是什么意思?我看电路中DVDD接的是TAS5760_DVDD,不是3.3V吗? DVDD这个引脚是内部数字电路的供电电压,包括控制引脚,比如SPK_SD, 它的电压也是参考DVDD。 内部LDO是通过AVDD供电,然后ANA_REG输出电压。
另外,没有输出的话,fault引脚输出什么电平? 看是否内部保护电路发生报错。
您好
1. 根据手册中下面的意思,DVDD是内部LDO供电,所以理论上AVDD供电后,DVDD应该就有3.3V电压输出了,但实际是没有电压输出;

2. 只要给PVDD上电12V,无论SPK_Shutdown pull-high or pull-low,也无论SPK_Shutdown与PVDD的先后时序,SPK_FAULT都=0.5V~0.7V一直不变,既不是high也不是low。给PVDD上电12V后,SPK_FAULT电压会花费几秒钟时间缓慢上升到0.5V~0.7V,然后保持不变.
请帮忙看看原因。
fault也是参考的DVDD,输出低电平的最大值为10%DVDD,所以DVDD这里没有电压输出,但是fault引脚还是有电压的,所以不正常的。
有更换新的IC试试吗?
TAS5760的架构图可以看出,DVDD需要外部供电啊,箭头向下,如果是输出,应该是和ANA_REG一样为输出:

另外,从上电时序的描述来看,PVDD, AVDD或者DVDD没有上电顺序,哪个先上电都没关系。

上图中您附上的DVDD的介绍来看,只说明内部LDO和DVDD连接的,ANA_REG为LDO的输出。
所以我理解的DVDD需要外部3.3V供电呢,您可以试试看是否能正常工作。
AVDD是加电压了,内部LDO输出到ANA_REG应该有电压吧?但是目前ANA_REG输出0V.
是的,ANA_REG应该是有输出的。
DVDD外加3.3V试试,是否有什么变化,等待您的反馈。
感谢您的反馈, 关于红色部分的意思,您误解了,它的上一句:
Some portions of the device also require a separate power supply which is a lower voltage than the DVDD supply. To simplify the power supply requirements for the system, the TAS5760M-Q1 device includes an integrated low-dropout (LDO) linear regulator to create this supply. This linear regulator is internally connected to the DVDD supply and its output is presented on the ANA_REG pin。
器件的某些部分需要单独的低于DVDD的供电电压,为了简化系统的供电需求,TAS5760内部包含一个LDO来建立这个电压(指的是上面提到的低于DVDD的给某些部分供电的电压)。LDO内部是和DVDD连接在一起的,其输出显示在ANA_REG引脚上。
所以从这里的描述来看,并不是LDO的输出电压是DVDD,只是说LDO内部和DVDD接在一起,输出呈现在ANA_REG引脚上。