This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5121: I2S三线方式输入时,BCK/DIN/LRCK这三线是否可以从GPIO口分别输出?

Part Number: PCM5121

I2S三线方式做从模式输入时,BCK/DIN/LRCK这三线是否可以从GPIO口分别输出?

DOUT好象可以配置从GPIO口输出,BCK/LRCK可以吗?

(不理解文档中说:主模式BCK/LRCK/BCK可以做输出,什么时候会用到这种场景?)

谢谢!

  • I2S三线方式做从模式输入时,BCK/DIN/LRCK这三线是否可以从GPIO口分别输出?

    DOUT好象可以配置从GPIO口输出,BCK/LRCK可以吗?

    您好,GPIO2和DOUT是复用引脚,DOUT是可以从GPIO2输出的,通过配置Page0 Register81 G2SL[4:0] 来选择GPIO2的输出,如下。BCK和LRCK是不可以的。

    主模式BCK/LRCK/BCK可以做输出,什么时候会用到这种场景?

    这里的意思是,PCM512可以工作在slave从机模式,也可以工作在主机maste让模式,当工作在master 模式时,LRCK或者BCK是输出引脚。

    如果工作在slave mode的话,这两个引脚作为输入,需要提供时钟输入。