42管脚是VCC,怎么接到了GND?
同时41管脚是GND,怎么接到了VCC呢?
是41,42管脚的定义错了,还是这个图画错了?
麻烦TI的FAE解答我这个问题,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好,谢谢,顺便问一句,DIX9211是否和PCM9211的DIE是一样的,启用那几个RSV,其实也有AD的功能?
你好,
还是有些差别的,DIX9211没有内置ADC,那几个引脚只是预留在那里。
你好,我在画电路图的时候,又遇到问题了:
1. 如果内置的S/PDIF AMP不使用(VCCRX = 0),那么如何处理RXIN1和RXIN2?需要通过电容接地吗?还是留着这两个管脚不接?
2. 如果RXIN2~RXIN7有不需要用的,应该如何处理?