Other Parts Discussed in Thread: TLV320AIC3101
最近在用HP8903B,做tlv320aic3101芯片的性能测试。为了测量芯片的SINAD参数,测试信号(正弦单音信号)由MIC2L单端输入.经由PGA、ADC、DACL,最后由HPROUT单端输出。出现的情况具体如下:
(1) 芯片的总增益为一定值K时,不用AGC,输入由小逐渐增大,输出亦由小增大,在输出小于700 mVRMS 的部分SINAD也增大,最大可达到50多dB,当输出大于700 mVRMS 时,输出信号出现削峰,此时SINAD急剧下降。
(2) 芯片的总增益为一定值K,通过对寄存器进行设置,将最终输出恒定设置为630 mVRMS 当输出随输入的增加,第一次到达630 mVRMS时,SINAD达到最优,但是之后输入一直增加,输出由于AGC的作用,在630 mVRMS左右,未出现削峰,且由示波器上未看到明显的噪声。但是SINAD急剧下降,且在30dB左右,或更低。具体的寄存器配置如下:
W30 0F 28 // L-PGA增益设定为20dB (reg 15)
W30 1A 9F // Left AGC enable, Target gain = -8db, Attack time = 20ms, decay time = 500ms(reg 26)
W30 1B 78 // Left AGC Maximum gain applicable = 30db(reg 27)
W30 1C 38 // Left AGC Hysteresis =1db, noise threshold = -84db(reg 28)
W30 22 7F // Left AGC Noise detect debounce = 512ms, signal debounce = 32ms(reg 34)
W30 3D 81 //DAC_L1 no routed to HPROUT Volume Control,音量=-0.5dB(reg 61)
其中,以下参数做过调整,但是结果还是一样
Target gain = -5.5 db~-12 db
Attack time = 8ms~20ms,Decay time = 100ms ~500ms
Noise threshold = -76db~ -90db
Maximum gain applicable =0db~32db
Hysteresis = 1db~3db
正常情况下,输入越大, SINAD参数会越好,所以不知道怎样才能在使用AGC效果的同时,保证SINAD参数的良好?具体应该调整哪些参数,如何调整?非常希望能够得到给位的帮助,谢谢!!