Other Parts Discussed in Thread: TPA3130D2
打算使用TPA3130D2去驱动AS05008PR-WR-R扬声器(8欧,1瓦rated),power supply大约5v恒压
TPA3130D2按datasheet所述,在5v驱动的情况下最大输出功率约为2.5瓦
如何知道实际输出功率会是多少?如何限制实际输出功率到1瓦?对于1瓦的扬声器来说是否有烧坏的危险?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPA3130D2
打算使用TPA3130D2去驱动AS05008PR-WR-R扬声器(8欧,1瓦rated),power supply大约5v恒压
TPA3130D2按datasheet所述,在5v驱动的情况下最大输出功率约为2.5瓦
如何知道实际输出功率会是多少?如何限制实际输出功率到1瓦?对于1瓦的扬声器来说是否有烧坏的危险?
你好:
功放的实际输出功率,可以在LCfilter之后,也就是负载上直接用万用表测量,P=U2/R,即知输出功率。
可以根据功放的放大倍数,限制前级的输入信号,才能限制输出为想要的值。
5V供电下,最大输出功率是1w多,需要限制前级输入,不给太大,即可。
多谢回复!
TPA3130D2的最小放大倍数为20dB,是否可以简单理解为输出电压是前级输入的10倍;输出功率为输入功率的100倍?
你好:
是的,输出电压是输入电压的10倍,输出功率实际上是把电源的功率转到输出这来了,总的功率是守恒的。
你可以采用上贴中提到的Plimit。
我感觉你可以理解为输出电压是前级输入的10倍(无失真情况下),但是输出功率为输入功率的100倍,这个貌似不太恰当。输出信号的功率只从TPA3130D2的电源汲取
不失真电压10倍没问题。
功率100倍不对。因为输入阻抗和输出阻抗不同。