This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用音频卡输出i2s接口数据,采集到的数值始终为0xffff,是我硬件电路设计的问题么?



求助问题分析思路

  • 不能排除, 非常可能. 还是先检查硬件比较简单, 包括焊接, 电源, 连线 等等因素.

  • 放大器没有问题,ad也有输出,串行输出高低电平,但是就是读到的数据是0xffff

  • 你好:

    可否详细描述你的问题,例如以下几点:

    1.应用场景

    2.系统框图

    3.硬件电路

    4.软件配置

    5.已经做过什么检查

     

  • 您好,新年快乐!

    我来描述一下各个问题,感谢您的解答

    1:应用于采集信号,信号电平大约在300mv左右的正弦信号。

    2:我采用ti的28069dsp作为主机采集ak5357vt(数据手册见附录) 输出的电平,总线是i2s,通过28069的mcbsp进行采集,其中主机生成了触发信号,主时钟,和串行数据时钟,从机输出采样后的高低电平信号输出。

    3:附录是我的硬件电路。

    4:附录附上我的软件配置,主要是mcbsp的配置。

  • 这个附录是我的软件设置

    void initmcbsp()
    {
    	EALLOW;
    	////////////////////////////////////
    	 McbspaRegs.SPCR1.bit.RRST=0; // Receiver reset
    	 McbspaRegs.SPCR2.bit.FRST=0;
    	 McbspaRegs.SPCR2.bit.GRST=0;
    	 //////////////////////////////////
    	 McbspaRegs.SPCR1.all=0x2000;
    	 McbspaRegs.RCR1.all=0x00A0;
    	 McbspaRegs.RCR2.all=0x80A6;
    	 McbspaRegs.SRGR1.all=0X219F;
    	 McbspaRegs.SRGR2.all=0x3041;
    	 McbspaRegs.SRGR1.bit.CLKGDV=5;
    	 McbspaRegs.PCR.bit.FSRM=1;
    	 McbspaRegs.PCR.bit.CLKRM=1;
    	 McbspaRegs.PCR.bit.CLKRP=1;
    	 McbspaRegs.PCR.bit.SCLKME=0;
    	  McbspaRegs.PCR.bit.FSRP=0;
    	 McbspaRegs.SRGR2.bit.FPER=65;
    	 McbspaRegs.SRGR1.bit.FWID=33;
    	 McbspaRegs.RCR1.bit.RFRLEN1=1;
    	 McbspaRegs.RCR2.bit.RFRLEN2=1;
    	 McbspaRegs.RCR2.bit.RPHASE=1;
    	 McbspaRegs.RCR1.bit.RWDLEN1=5;
    	 McbspaRegs.RCR2.bit.RWDLEN2=5;
    	 McbspaRegs.RCR2.bit.RFIG=1;
    	 McbspaRegs.RCR2.bit.RCOMPAND=00;
    	 McbspaRegs.RCR2.bit.RDATDLY=01;
    	McbspaRegs.SPCR1.bit.RJUST=0x00b;
    	McbspaRegs.SPCR1.bit.RRDY=0;
    	 McbspaRegs.PCR.bit.CLKRP=0;
    
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP ");  
    	McbspaRegs.SPCR2.bit.FREE=1;
    	McbspaRegs.SPCR2.bit.SOFT=0;
    	McbspaRegs.SPCR2.bit.GRST=1;
    	McbspaRegs.SPCR1.bit.RRST=1;
    	McbspaRegs.SPCR2.bit.FRST=1;
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP ");
    	
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP ");  
    	 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP "); 
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP ");
    	 // Receiver reset
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP ");  
    	EDIS;
    	asm (" NOP ");
    	asm (" NOP ");      // Wait at least 2 SRG clock cycles
    	asm (" NOP ");  
    }
  • 这个附录是我所采用的ad芯片数据手册

    AK5357VT.pdf
  • 目前从串行数据看,到ad输出这一部分没有问题,但是为何drr寄存器中的值始终为0xffff,不得而知!~!!!!!!!!

  • 你好:

    建议检查DSP的方面的软件配置,阅读AK5357的数据手册检查问题。

    很抱歉AK5357不是TI的产品,我也不是很熟悉。

     

     

  • 这位老师,我看你回答了好多帖子的问题特别热心,能在这里问你个问题吗?问题如下,请帮忙解决

    我用的板子是TMS320VC5509A,我想用它来采集声音信号,在官方提供的第27个例子中,连接电脑能听到电脑播放的音乐,如果我想在输入口接个麦克风采集声音信号,该怎么处理呢?直接用这个程序能不能实现,我用的是虚拟机XP系统,我现在直接用程序的话,感觉麦克风不起作用,运行后有噪音,这个是什么问题我该怎么解决?

    程序如下:#include <csl.h>
    #include <csl_i2c.h>
    #include <stdio.h>
    #include <csl_pll.h>
    #include <csl_mcbsp.h>

    #define CODEC_ADDR 0x1A


    /*锁相环的设置*/
    PLL_Config  myConfig      = {
      0,    //IAI: the PLL locks using the same process that was underway
                    //before the idle mode was entered
      1,    //IOB: If the PLL indicates a break in the phase lock,
                    //it switches to its bypass mode and restarts the PLL phase-locking
                    //sequence
      12,    //PLL multiply value; multiply 24 times
      1             //Divide by 2 PLL divide value; it can be either PLL divide value
                    //(when PLL is enabled), or Bypass-mode divide value
                    //(PLL in bypass mode, if PLL multiply value is set to 1)
    };


    MCBSP_Config Mcbsptest;
    /*设置McBSP,使用McBSP1来发送和接收来自DSP 和 AIC23的数据*/
    /*McBSP set,we use mcbsp1 to send and recieve the data between DSP and AIC23*/
    MCBSP_Config Mcbsp1Config = {
      MCBSP_SPCR1_RMK(
        MCBSP_SPCR1_DLB_OFF,                   /* DLB    = 0,禁止数字回环方式 */
        MCBSP_SPCR1_RJUST_LZF,                 /* RJUST  = 2 接收数据符号扩展和调节方式*/
        MCBSP_SPCR1_CLKSTP_DISABLE,            /* CLKSTP = 0 */
        MCBSP_SPCR1_DXENA_ON,                  /* DXENA  = 1 DX引脚延时使能打开*/
        0,                                     /* ABIS   = 0 */
        MCBSP_SPCR1_RINTM_RRDY,                /* RINTM  = 0 接收中断模式*/
        0,                                     /* RSYNCER = 0 接收帧同步错误标志*/
        MCBSP_SPCR1_RRST_DISABLE               /* RRST   = 0 禁止接收器复位*/
       ),
        MCBSP_SPCR2_RMK(
        MCBSP_SPCR2_FREE_NO,                   /* FREE   = 0 */
        MCBSP_SPCR2_SOFT_NO,                   /* SOFT   = 0 */
        MCBSP_SPCR2_FRST_FSG,                  /* FRST   = 0 帧同步逻辑复位 */
        MCBSP_SPCR2_GRST_CLKG,                 /* GRST   = 0 采样率发生器复位 */
        MCBSP_SPCR2_XINTM_XRDY,                /* XINTM  = 0 发送中断模式*/
        0,                                     /* XSYNCER = N/A */           
        MCBSP_SPCR2_XRST_DISABLE               /* XRST   = 0 发送器复位*/
       ),
       /*单数据相,接受数据长度为16位,每相2个数据*/
      MCBSP_RCR1_RMK(
              MCBSP_RCR1_RFRLEN1_OF(1),              /* RFRLEN1 = 1 接收阶段1的帧长为1个字 */
              MCBSP_RCR1_RWDLEN1_16BIT               /* RWDLEN1 = 2 接收阶段1的字长为16位 */
      ),
      MCBSP_RCR2_RMK(   
        MCBSP_RCR2_RPHASE_SINGLE,              /* RPHASE  = 0 接收帧的阶段数*/
        MCBSP_RCR2_RFRLEN2_OF(0),              /* RFRLEN2 = 0 接收阶段2关闭*/
        MCBSP_RCR2_RWDLEN2_8BIT,               /* RWDLEN2 = 0 接收阶段2的字长为8位*/
        MCBSP_RCR2_RCOMPAND_MSB,               /* RCOMPAND = 0 接收数据压扩模式*/
        MCBSP_RCR2_RFIG_YES,                   /* RFIG    = 0  忽略不期望接收的帧同步信号 */
        MCBSP_RCR2_RDATDLY_1BIT                /* RDATDLY = 1 接收数据延时*/
        ),  
       MCBSP_XCR1_RMK(   
        MCBSP_XCR1_XFRLEN1_OF(1),              /* XFRLEN1 = 1 发送阶段1的帧长(一个)*/
        MCBSP_XCR1_XWDLEN1_16BIT               /* XWDLEN1 = 2 发送阶段1的字长16位*/
       
    ),   
    MCBSP_XCR2_RMK(   
        MCBSP_XCR2_XPHASE_SINGLE,              /* XPHASE  = 0 */
        MCBSP_XCR2_XFRLEN2_OF(0),              /* XFRLEN2 = 0 */
        MCBSP_XCR2_XWDLEN2_8BIT,               /* XWDLEN2 = 0 */
        MCBSP_XCR2_XCOMPAND_MSB,               /* XCOMPAND = 0 */
        MCBSP_XCR2_XFIG_YES,                   /* XFIG    = 0 */
        MCBSP_XCR2_XDATDLY_1BIT                /* XDATDLY = 1 发送数据延时*/
      ),            
    MCBSP_SRGR1_DEFAULT,
    MCBSP_SRGR2_DEFAULT,  
    MCBSP_MCR1_DEFAULT,
    MCBSP_MCR2_DEFAULT,
    MCBSP_PCR_RMK(
       MCBSP_PCR_IDLEEN_RESET,                 /* IDLEEN   = 0   */
       MCBSP_PCR_XIOEN_SP,                     /* XIOEN    = 0   */
       MCBSP_PCR_RIOEN_SP,                     /* RIOEN    = 0   */
       MCBSP_PCR_FSXM_EXTERNAL,                /* FSXM     = 0   */
       MCBSP_PCR_FSRM_EXTERNAL,                /* FSRM     = 0   */
       0,                                      /* DXSTAT = N/A   */
       MCBSP_PCR_CLKXM_INPUT,                  /* CLKXM    = 0   */
       MCBSP_PCR_CLKRM_INPUT,                  /* CLKRM    = 0   */
       MCBSP_PCR_SCLKME_NO,                    /* SCLKME   = 0   */
       MCBSP_PCR_FSXP_ACTIVEHIGH,              /* FSXP     = 0   */
       MCBSP_PCR_FSRP_ACTIVEHIGH,              /* FSRP     = 1   */
       MCBSP_PCR_CLKXP_FALLING,                /* CLKXP    = 1   */
       MCBSP_PCR_CLKRP_RISING                  /* CLKRP    = 1   */
    ),
    MCBSP_RCERA_DEFAULT,
    MCBSP_RCERB_DEFAULT,
    MCBSP_RCERC_DEFAULT,
    MCBSP_RCERD_DEFAULT,
    MCBSP_RCERE_DEFAULT,
    MCBSP_RCERF_DEFAULT,
    MCBSP_RCERG_DEFAULT,
    MCBSP_RCERH_DEFAULT,
    MCBSP_XCERA_DEFAULT,
    MCBSP_XCERB_DEFAULT,
    MCBSP_XCERC_DEFAULT,
    MCBSP_XCERD_DEFAULT,  
    MCBSP_XCERE_DEFAULT,
    MCBSP_XCERF_DEFAULT,  
    MCBSP_XCERG_DEFAULT,
    MCBSP_XCERH_DEFAULT
    };   
    /*创建和初始化I2C模块*/  
    /* This next struct shows how to use the I2C API */
    /* Create and initialize an I2C initialization structure */
    I2C_Setup I2Cinit = {
            0,              /* 7 bit address mode */
            0,         /* own address - don't care if master */
            84,            /* clkout value (Mhz)  */
            50,            /* a number between 10 and 400*/
            0,              /* number of bits/byte to be received or transmitted (8)*/
            0,              /* DLB mode on*/
            1               /* FREE mode of operation on*/
    };

    I2C_Config testI2C;


    /*数字音频接口格式设置
    AIC23为主模式,数据为DSP模式,数据长度16位*/   
    Uint16 digital_audio_inteface_format[2]={0x0e,0x53};
    /*AIC23的波特率设置,采样率为44.1K*/
    Uint16 sample_rate_control[2] = {0x10,0x23};
    /*AIC23寄存器复位*/
    Uint16 reset[2] ={0x1e,0x00};
    /*AIC23节电方式设置,所有部分均所与工作状态*/
    Uint16 power_down_control[2] ={0x0c,0x03};

    /*AIC23模拟音频的控制
    DAC使能,ADC输入选择为Line*/
    Uint16 analog_aduio_path_control[2] ={0x08,0x10};
    /*AIC23数字音频通路的控制*/
    Uint16 digital_audio_path_control[2] ={0x0a,0x05};
    /*AIC23数字接口的使能*/
    Uint16 digital_interface_activation[2] ={0x12,0x01};
    /*AIC23左通路音频调节*/
    Uint16 left_line_input_volume_control[2] ={0x00,0x17};
    /*AIC23右通路音频调节*/
    Uint16 right_line_input_volume_control[2] ={0x02,0x17};
    /*AIC23耳机左通路音频调节*/
    Uint16 left_headphone_volume_control[2] ={0x05,0xFF};
    /*AIC23耳机右通路音频调节*/
    Uint16 right_headphone_volume_control[2] = {0x07,0xFF};
    /*定义McBSP的句柄*/
    MCBSP_Handle hMcbsp;

    Uint16 i2c_status;
    Uint16 i,temp;

    void delay(Uint32 k)
    {
       while(k--);
    }


    void main(void)
    {

        Uint16 aic23data = 0;
            i2c_status = 1;
        /* Initialize CSL library - This is REQUIRED !!! */
        /*初始化CSL库*/
        CSL_init();
           
            /*设系统的运行速度为140MHz*/
        PLL_config(&myConfig);
       
        /* Initialize I2C, using parameters in init structure */
        /*初始化I2C的格式*/

    //        I2C_config(&Config);
    //        I2C_start();
           
    //        I2C_getConfig(&Config1);
            /*I2C is undet reset*/
            I2C_RSET(I2CMDR,0);
            /*设置预分频寄存器,I2C的mode clock is 10MHz*/
            delay(100);
            I2C_RSET(I2CSAR,0x001A);
            I2C_RSET(I2CMDR,0x0620);
                   
        I2C_setup(&I2Cinit);
              /*设置I2C的Mater clock*/
            I2C_RSET(I2CCLKL,100);
            I2C_RSET(I2CCLKH,100);

        I2C_getConfig(&testI2C);

            /*初始化McBSP0*/
            hMcbsp = MCBSP_open(MCBSP_PORT1,MCBSP_OPEN_RESET);
            /*设置McBSP0*/
            MCBSP_config(hMcbsp,&Mcbsp1Config);
            /*启动McBSP0*/
            MCBSP_start(hMcbsp,
                    MCBSP_RCV_START | MCBSP_XMIT_START,
                    0);

        MCBSP_getConfig(hMcbsp,&Mcbsptest);

        /*reset AIC23*/
        i2c_status = I2C_write( reset,          //pointer to data array  指向发送数据的数组
                                        2,                                //length of data to be transmitted  发送数据的长度16位
                                        1,                                //master or slaver   主模式
                                        CODEC_ADDR,            //slave address to transmit to 从地址发送
                                        1,                                //transfer mode of operation 传输模式
                                        30000                        //time out for bus busy    延时
                                            );
            delay(1000);
        /*设置AIC23各部分均工作*/
        i2c_status = I2C_write( power_down_control,//pointer to data array    省电控制
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                            );            
            /*设置AIC23的数字接口*/
            i2c_status = I2C_write( digital_audio_inteface_format,//pointer to data array 数字音频格式
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                               );
             /*设置AIC23模拟通路*/
    /*        i2c_status = I2C_write( analog_aduio_path_control,//pointer to data array  模拟音频格式
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                            );*/
            /*设置数字通路*/
            i2c_status = I2C_write( digital_audio_path_control,//pointer to data array 数字音频通路控制
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                              );           
            /*设置AIC23的采样率*/
            i2c_status = I2C_write( sample_rate_control,//pointer to data array     采样速率
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                        );
            /*设置耳机音量*/
            i2c_status = I2C_write( left_headphone_volume_control,//pointer to data array 耳机左声道音量调节
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                        );
            i2c_status = I2C_write( right_headphone_volume_control,//pointer to data array  耳机右声道音量调节
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                        );  
            /*设置Line输入的音量*/
            i2c_status = I2C_write( left_line_input_volume_control,//pointer to data array  左声道音量调节
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                        );
            i2c_status = I2C_write( right_line_input_volume_control,//pointer to data array  右声道音量调节
                                        2,                                //length of data to be transmitted
                                        1,                                //master or slaver
                                        CODEC_ADDR,            //slave address to transmit to
                                        1,                                //transfer mode of operation
                                        30000                        //time out for bus busy
                                        );
            /*启动AIC23*/
            i2c_status = I2C_write( digital_interface_activation,//pointer to data array  数字接口激活
                           2,                                //length of data to be transmitted
                           1,                                //master or slaver
                           CODEC_ADDR,            //slave address to transmit to
                           1,                                //transfer mode of operation
                           30000                        //time out for bus busy
                           );
                          
            /*回放音频*/
            while(TRUE)
            {
                    while(!MCBSP_rrdy(hMcbsp)){};
                    aic23data = MCBSP_read16(hMcbsp);
                    MCBSP_write16(hMcbsp,aic23data);      
                }
    }

    还有就是,我要先看声音信号的图,那么我的开始地址应该设为哪个参数呢?这个程序的输入数据在什么地方体现?