This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1641: OPA164X运放输出异常

Part Number: OPA1641


故障描述:

OPA164X  为IN-轨对轨器件,双电源宽电压,其中最低供电电压为±2.5V。但实际仿真和实测发现,器件在±2.5V供电时无法正常工作。由于目前OPA164X仍有几千的库存量,这导致我们无法使用。请求TI相关技术人员帮忙寻求下原因。

  • 您好,

    如下输入共模电压范围规格截图,±2.5V供电的话,输入范围是-2.6V ~ -1V,您仿真输入的0.5V不在这个输入共模范围内,因此输出异常,您输入-2.6V ~ -1V这个范围内的信号,测试正常吗?