This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3120: 8kHz采样率时,无法设置输出格式为16bit,必须设置为32bit

Part Number: TLV320ADC3120

在调试TLVADC3120时,器件配置:外部16MHz MCLK时钟输入,只配置左声道输出,当采样率设置为8kHz和16bit,I2S总线上没有输出数据,配置为8kHz和32bit,I2S总线上可以读取数据,但配置为其它的采样率如16kHz和16bit也可以在I2S上读取到数据,以上读取数据使用逻辑分析仪测试

  • 当采样率设置为8kHz和16bit,I2S总线上没有输出数据,配置为8kHz和32bit,I2S总线上可以读取数据

    只配置左声道,根据MCLK=BCLK*channel number*fs可以计算 BCLK=16M/8Khz*1=0.2Mhz

    参考Table 8-6和8-7的表格,ADC3120可以配置为各种各样的采样速率,BCLK的最小频率为0.256Mhz,所以当BCLK/FSYNC的比值为16或24的时候是reserved状态。

  • 如果将MCLK时钟降低到8MHz,是不是就可以了

  • 我上面的MCLK公式应该写错了。我觉得您同时采集左右两个通道应该就可以了。

    应该是: 位时钟BCLK= 通道数*采样速率*位宽

    因为目前您只采集左声道,所以8Khz,16bit位宽 BCLK=0.128Mhz,如果同时采集左右两个通道,那么BCLK=2*8Khz*16bit=0.256Mhz.