用来前级放大50倍的芯片,频率2KHZ-15KHZ之间,要求噪声平稳,本人水平有限,最好可以单电源锂电池供电,电路要求不太高的,价格不考虑,暂时用的是LM386效果不是很理想,求推荐。以及滤波器的相关推荐
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
1.放大音频的滤波器运放,建议采用双电源供电,因为音频信号是有正有负的。双电源供电的运放,性能也更有。
2.电源轨也是能用宽范围就用宽电源轨,否则不能达到最好的性能。
3.如果实在不方便用宽电源轨,也没有负电的,可以用TPS65135,TPS65132等芯片转成+5V,-5V给运放供电。
4.运放可以推荐用LM4562,这个运放的指标比较好,低噪声,SNR和THD+N都比较好。
5.运放的滤波器架构连接,可以连接成1阶的也可以连接成2阶的,butterworth或者Mutil feedback的都可以。