This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: 按默认配置,无输出,无PLL_LOCK

Part Number: CDCE62005

采用AUX_IN输入25MHz时钟,外部配置引脚如图均设为高电平(经测量确为高电平),芯片寄存器为默认,希望能实现芯片手册示例中的输出(156.25MHz和125MHz等输出)。

经测量芯片供电正常,输入时钟正确给入,但都无输出,且PLL_LOCK始终为低电平。求问可能是出了什么问题?

  • 您好,

    我不确定是不是与这个有关,datasheet 描述AUX IN输入需要接晶振,您可以试一下改将输入时钟接至Primany 输入或是 secondary 输入管脚,看输出有没有变化?

    另外,您是否可以写一下VCO校准位, 因为如果VCO校准不启动,将不会有任何输出: