阅读了ADS1675参考原理图发现一个疑问,请教。
ADS1675的CLK的管脚采用SN74AHC1G32DRL接入时钟,时钟源为CY22393产生。但是看了一下这个两个器件的手册,感觉电压不匹配。
SN74AHC1G32DRL在5.5v供电时,输入高最小电压为3.85V;而CY22393为3.3v供电,不可能产生这个最小电压。
请问这个是什么情况?或者SN74AHC1G32DRL在5V供电的时候能行?(手册里面没有明示啊)
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
阅读了ADS1675参考原理图发现一个疑问,请教。
ADS1675的CLK的管脚采用SN74AHC1G32DRL接入时钟,时钟源为CY22393产生。但是看了一下这个两个器件的手册,感觉电压不匹配。
SN74AHC1G32DRL在5.5v供电时,输入高最小电压为3.85V;而CY22393为3.3v供电,不可能产生这个最小电压。
请问这个是什么情况?或者SN74AHC1G32DRL在5V供电的时候能行?(手册里面没有明示啊)
谢谢
SN74AHC1G32DRL是可以5V供电的。
但是你说的是对的,如果想输出高电平Vcc,至少要满足VIh,Vil的要求。
这里看起来使用SN74AHC1G32是不正确的。
你好,我需要用两颗ADS1675同步采样,ADS1675时钟的VIH要求为0.7*AVDD(AVDD=5V);
我采用CY2304NZ作为时钟buffer,CY2304NZ的供电压为3.3V。
1、是否能推荐一片逻辑芯片实现CY2304NZ到ADS1675的电平转换;
2、能否推荐一片2个时钟输出的时钟buffer了,能够连接到ADS1675?
3、如果都比较困难,是否能够采用5V的晶振,通过菊花链的方式将时钟输给两颗ADS1675?
谢谢您!
实际上电平变换大多利用74系列的成本较低,这里的确不太恰当;但是你要考虑74芯片会有输入容性,3.3V会被寄生电容的响应拉高即产生一个上冲,会超过HI,之后只要不低于LI就好了;也算合理、稳定。
较高成本的buffer的时钟附加抖动会很小,多采用回滞比较器输入、PLL+差动输出。(一定要的话可以试一下高速比较器:TLV3502 / TLV3501并需要添加回滞电阻)
作为一个才4M的器件,只是提供采样震荡,没必要这么干
所以推荐你74lvc2g14或74lvc2g32,接同一输入源(效果更好)即可
是否能推荐一片逻辑芯片实现CY2304NZ到ADS1675的电平转换;
A: 可以采用AHCT系列的,比如SN74AHCT1G125,可以实现3.3V到5V的切换。