This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:选择合适的AD和DA评估板。可以帮忙找一下吗?谢谢!

Other Parts Discussed in Thread: DAC3161, ADS4126

要求如下:

1.选定满足指标(位数:12位;采样率:150MSPS)的AD和DA芯片评估板,要求所选定的AD和DA评估板可以配套使用。

2.选定AD和DA评估板,分别给出以下内容:

① AD和DA评估板型号和所在官网链接

② 评估板的官方价格

③ 评估板的接口特性,即对于AD评估板,指出它是如何将数字信号传给PC的;对于DA评估板,指出它是如何与PC端口连接的。给出文档原文内容。

  • 需要几个通道的?单通道的话AD可以参考ADC4126,12bit, 160MSPS采样率。

    DA的话可以参考DAC3161,采样率最高500MSPS。

  • 评估板链接,http://www.ti.com/tool/dac3161evm

     http://www.ti.com/tool/ADS4126EVM

    ADS4126可以配置成LVDS或CMOS输出,DAC3161是LVDS输入。

  • 谢谢您!我想补充问一下: 我要买的是双通道的,根据您的建议,我看了一下AD的可以是ADS4126, DA的可以是DAC3161。

    这里还有两个问题:

    (1)如果直接在官网上购买这两个评估板的话,这两个评估板是包括了所有套件吗?即买回来之后就可以直接用的,比如对于ADS4126这个评估板,买回来之后给定一个模拟信号就可以了,然后通过这个评估板就可以输出数字信号,再通过LVDS或CMOS给PC,是这样的吗?

    (2)你所说的“ADS4126可以配置成LVDS或CMOS输出,DAC3161是LVDS输入。”这个具体是通过什么与PC连接了?

    谢谢!

  • 谢谢您!我想补充问一下: 我要买的是双通道的,根据您的建议,我看了一下AD的可以是ADS4126, DA的可以是DAC3161

    这里还有两个问题:

    (1)如果直接在官网上购买这两个评估板的话,这两个评估板是包括了所有套件吗?即买回来之后就可以直接用的,比如对于ADS4126这个评估板,买回来之后给定一个模拟信号就可以了,然后通过这个评估板就可以输出数字信号,再通过LVDS或CMOS给PC,是这样的吗?

    (2)你所说的“ADS4126可以配置成LVDS或CMOS输出,DAC3161是LVDS输入。”这个具体是通过什么与PC连接了?

    谢谢!