This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: 使用ads1299evm外接mcu开发时,spi信号会干扰到AGND

Part Number: ADS1299


您好!我使用MCU的5V,3.3V和GND为ADS1299EVM供电和接地(对应EVM的5V,3v3和DGND),我每隔150ms读取16ms数据。下图是示波器探针在交流耦合的设置下测量EVM的5V和AGND得到的。从示波器的图像中可以看到在读取的时候(也就是每150ms的开头16ms),有大量的噪声干扰,这会影响到我的数据采集(叠加之后会有一个较为严重的伪迹),这个问题为什么会出现以及我该如何解决这个问题image.png