Other Parts Discussed in Thread: DAC1280
我想请问下关于DAC1280的TDATA引脚输入的比特流的问题:
1,怎么产生这个比特流,算法是什么?
2,怎么控制输出信号的频率?
对您的回答感激不尽,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DAC1280
我想请问下关于DAC1280的TDATA引脚输入的比特流的问题:
1,怎么产生这个比特流,算法是什么?
2,怎么控制输出信号的频率?
对您的回答感激不尽,谢谢。
TDATA is the digital signal input and determines the output frequency and amplitude. TDATA is encoded as a 1s density bitstream where the DAC1280 output is proportional to the 1s density. When the 1s density input is 75% (that is, on average, three out of four TDATA bits are '1'), the differential output current is at a positive maximum value; when the 1s density input is at 25% (on average, three out of four TDATA bits are '0'), the differential output current is at a negative maximum value. When the 1s density is 50% (on average, an equal number of '1's and '0's), the differential output current is 0. See Table 1.
这里说了高电平的密度, 可以看作是 PWM 脉宽的另一个说法
你好~!
我看了这一段,说是可以控制振幅和频率,可是频率怎么控制我没看太懂,能大概解释一下吗?
我打个比方,上面说0输出是50%的高电平密度, 那么假设4个比特位 ,1100和1010还有1001都是50%的高电平密度 难道输出一样吗
谢谢