This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298R的 PACE 功能?

PACE_OUT1和PACE_OUT2这两条引腿究竟是输入还是输出?有什么用?怎样使用?

  • 你好!

    PACE_OUT1和PACE_OUT2这两个引脚可以作为复用的差分输入,或者内部pace detection的信号测试点。总体来说,这两个就是测试信号点,主要通过通过设置寄存器,这两个引脚可以获得芯片内部pace_out前的某一点的信号,当然也可以输入差分信号来测试后续的电路的性能。

    当然这两个引脚是一般在实际的电路是可以不使用的,可以将其作为测试点使用。

    具体的可以参照page23的” Test Signals (TestP and TestN)”,以及page68和page69有详细的使用说明。

  • 顺便问一下,能否简述一下你的应用场景。