Other Parts Discussed in Thread: ADS1246
ADS1246最大数据输出速率是2ksps。
1.如果我的信号频率范围是1Hz到700Hz。ADS1246能否满足信号完整输出?
2.如果每采集完一个点,进行一次带通滤波,在用MATLAB生成滤波系数的时候,其中采样频率fs与AD的采样率或者数据输出速率有关联吗?这个采样频率fs有受限制吗?
麻烦啦。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1246
ADS1246最大数据输出速率是2ksps。
1.如果我的信号频率范围是1Hz到700Hz。ADS1246能否满足信号完整输出?
2.如果每采集完一个点,进行一次带通滤波,在用MATLAB生成滤波系数的时候,其中采样频率fs与AD的采样率或者数据输出速率有关联吗?这个采样频率fs有受限制吗?
麻烦啦。
你好:
1.这主要由内部数字滤波决定,不同速率下不一样,具体请看手册30页,Table 10. Digital Filter Specifications,以及P31,32的相关图形。
2. 你所说的Fs应该就是采样速率。
Hi,你好:
请教一下。1.ADS1246能满足20Hz-500Hz的带宽输入要求吗?
2.如果能满足,那么当采集完再进行20Hz-500Hz的数字带宽滤波,波形能完整输出吗?
1.模拟部分可以的;
2.你说进行20Hz-500Hz的数字带宽滤波是指在哪儿滤?如果是adc内部的话还请你看下手册31,32的图形来选择你需要的速率,谢谢。