This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1274+THS4521 能否采集更宽的电压范围

Other Parts Discussed in Thread: THS4521, ADS1274

目前使用ADS1274+THS4521做压力方面的应用,2.5V的ommon-mode input voltage (VCM),实际测试时发现,我们1mV的压力代表十几个内码数。

A   请问ADS1274是否最大就支持2.5V的ommon-mode input voltage (VCM)的,如果能支持更大的话,我们可以让1mV的压力代表的内码数值降低,相应的精度会提高。

B   请问,如果ADS1274的参考电压VREFP如果使用REF5030-3.0V,而VCOM还是2.5V接到THS4521,会有什么影响吗,其它不变的情况下,测试精度是否会有改善?

  • A.  ADS1274是差分输入,VCM的设置不会直接影响可接受的差摸输入范围(- Vref到 + Vref),只要保证输入pin脚上的范围从(Vcm - Vref/2到 Vcm + Vref/2)不超过0V到AVDD。所以对于ADS1274+THS4521,AVDD用5V,配置VCM为2.5V是合理的。

    B.增加ADC输入范围,提高运放的放大倍数,可以改善精度。