Other Parts Discussed in Thread: ADS5562
1、用FPGA配置ADS5562怎么确认寄存器是否配置正常
2、输入时钟和输出时钟的延时怎样配置在合理的范围里
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
分别使能Reset,Power down和Test Pattern寄存器
看看ADC有正确的响应没有
这些信号都是正常的,配置寄存器时序也没什么问题,基准电压用了内部基准,输入信号为1.42V,AD输出为0x9335,用二进制补码形式输出