Other Parts Discussed in Thread: ADS1262
最近我在使用ADS1262,我现在采用的是四线和MCU进行通讯,分别是CS,SCLK,DIN,DOUT和MCU进行接口,请问这样是否可以?我看手册中不是说开启转换可以通过两种方式,一种是让START为高,另外一种是发送START命令?难道非得再加上一根START线才能进行启动转换吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1262
最近我在使用ADS1262,我现在采用的是四线和MCU进行通讯,分别是CS,SCLK,DIN,DOUT和MCU进行接口,请问这样是否可以?我看手册中不是说开启转换可以通过两种方式,一种是让START为高,另外一种是发送START命令?难道非得再加上一根START线才能进行启动转换吗?
从手册看, START 命令和 START 信号具有相同的效果, 你可以使用 START 命令
ADC1 conversions are controlled by the START pin or by serial commands. If using commands to control ADC1 conversions, keep the START pin low to avoid possible contentions between the START pin and commands.
不过我看还是最好能先验证一下
这一段中的确是说使用START命令和使用START引脚效果都是一样的,但他在此段中也说为了保证引脚和命令的不冲突,建议使用命令操作时把START引脚设置为低电平。
但在终止连续转换模式的那段中也说了,在START引脚上置低会终止连续转换模式,
这样给我的感觉是貌似并不能讲start引脚单纯的置为某一固定电平,应该可控才对?