Other Parts Discussed in Thread: LMX2581, LMK04906
本人想测试一款理论位数为16位的ADC,实际可能达到的有效位数在14位左右,实验室有一款安捷伦的信号源,我也不知道是否符合要求,想请教一下,要想精度方面不出现问题,信号源的参数大概应该在什么样的标准。又或者说如果这个信号源精度不够,有没有什么替代方案可以帮我完成测试。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的工程师:您好,我把信号源输入的正弦波信号通过带通滤波器,然后利用频谱分析仪得到SNR大概只有65~70dB,这样的话,我是否需要更换一个信号源,你说的精度上多两位,是比理论值多2位,还是比有效位数多两位?信号源精度如果不够,我除了更换一个信号源,还有没有其他办法
您好,由于我模拟输入的带宽设计的比较小,大概只有几十K,因此我把RBW设置的和实际带宽差不多25K左右,VBW的话在2.5K,span的话,设置的是0~50KHz,然后信号源的SNR并不高,如果用于测试估计精度不够,不知道有没有什么其他的方式可以提高信号源精度,又或者是我频谱分析仪使用的时候有错误?