This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293的I、II、III三导联能够出来,增强导联aVR、aVF、aVL波形都出不来

名称

register

CMD

说明

WILSON_CN

0X10

0X02

Goldberger reference outputs internally connected to IN4, IN5 and IN6

WILSON_EN1


0X0D

0X01

First buffer amplifier connected to input IN1

WILSON_EN2


0X0E

0X02

Second buffer amplifier connected to input IN2

WILSON_EN3

0X0F

0X03

Third buffer amplifier connected to input IN3

FLEX_CH1_CN

0X01

0X0C

aVR ECG1:IN1-IN4

FLEX_CH2_CN

0X02

0X15

aVL ECG2:IN2-IN5

FLEX_CH3_CN

0X03

0X1E

aVF ECG3:IN3-IN6

CH_CNFG

0X2F

0x70

Configure Channel for Loop Read Back Mode

请帮我看看,配置是否有问题  ,谢谢