Other Parts Discussed in Thread: LMK04906, LMK03806, LMK04002, LMK02002, CDCE62002
大家好,我的ADC32XX 采样率为125M,将转换后的数据发送给FPGA,请问ADC32xx的时钟由FPGA直接输出吗?FPGA IO口是3.3V的,如果是这样的话是不是得电平转换一下,速率能保证吗?是否有更好的方法给出这个时钟呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADC的采样时钟一定不能由FPGA生成
FPGA生成的时钟性能太差。不能满足要求
看看专业时钟芯片LMK04906,LMK03806
你好,LMK04002怎么样,还有一个CLKout2不需编程上电就可输出固定频率,这样可以供给FPGA,FPGA再对LMK04002编程输出给ADC3K,这样可行吧?谢谢。
你好,LMK4096有6路输出,而我只用到一路给ADC,至多再有一路给FPGA,其他都没有用到,并且占用到FPGA I/O有8个,能否推荐一款适合这个ADC3K,并占用FPGA I/O较少的时钟芯片,最好也能给FPGA提供时钟的。谢谢!
如果对性能要求较高,LMK040xx和LMK041xx是比较好的选择, LMK02002则简单一些,性能也不错。如果成本系统简化要求则CDCE62002。