ADS1256我之前是使用6N137高速光耦进行隔离的,但是单片机控制继电器的时候有时会出现复位(继电器使用独立的开关电源供电,这个继电器控制AC电磁阀)。使用示波器探头夹在ADS1256的SCLK引脚,继电器工作2-3次就复位了。
如果我初始化ADS1256不给它发送SCLK信号,单片机不停的控制继电器的吸合断开,这样工作2个小时,然后再对ADS1256发送SCLK信号时发现(给它发SCLK信号时,需要进行一次自校准,不然AD值跳动有点大),ADS1256没有出现复位,工作正常;
请TI专家给我看看是不是隔离导致ADS1256复位的,使用ISO7241进行隔离最好是用哪个型号?