Other Parts Discussed in Thread: ADS7818, ADS7822
请问ADS7818可以用3.3V供电吗?手册上说要用5V,但是我以前朋友用了3.3V也可以工作,请工程师帮我确认是否可以用3.3V供电,因为我需要拿它的输出接3.3V的FPGA,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册上的各项指标都是按照+5V供电来的,同时有写明供电范围是4.75~5.25V。
如果一定要在3.3V下跑,芯片不会有问题,但是不保证性能。详见手册第三页左上角的表格,VCC到GND的电压可以从-0.3到6V。在3.3V下用时,注意输入信号范围不要超过3.3V。