This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900EVM开发板包含哪些工具,是否包含USB2ANY?请TI专家协助!!!!!!

Other Parts Discussed in Thread: USB2ANY, PGA900, PGA300

本人想购买一块PGA900EVM开发板,看到官网说需要使用USB2ANY编程,害怕买的板子不包含编程器,请问是否包含USB2ANY或OWI编程器?OWI编程器有什么推荐型号?

由于本人第一次做这个东西,不是很清楚。

请各位专家协助!!!!!!

  • 手册上这样所的:

    5 XDS200 and USB2ANY Connectors
    The XDS200 is used for the single-wire debugging (SWD) feature of the PGA900. The designer must use a small breakout board (part of the XDS200 kit) to connect to J17 in the PGA900EVM-034. No external connections are needed. Figure 10 shows the proper connection for the XDS200 emulator.

    这个板的组件

    The PGAxxxEVM-034 is divided into six sections:
    1. Interface boards and external power:
    (a) USB2ANY connector
    (b) XDS200 connector (single wire debugger)
    (c) Banana connectors to power up EVM
    2. Power:
    (a) 7.5-V, 5-V, and 3.3-V regulators
    3. Mode selection:
    (a) 4- to 20-mA loop (current mode)
    (b) Voltage mode
    4. OWI circuitry
    5. Resistive bridge
    6. Application components

    好象并没有提供 XDS200 和 USB2ANY, 这两个可能需要另外购买

  • 包含USB2ANY啊,可以看下EVM user's guide Page2中EVM板的图片,注明包含哪几部分了呢。

  • 你好,那个是这个板子的USB2ANY接口。

  • 如果支持评测PGA300的功能和性能,采购标准套件就够用了。要是你处还想实现对PGA900的编程开发,你还需要准备以下物件。

    1. XDS200仿真器

    2. CCS软件

    在CCS环境下完成代码开发后,可以通过PGA900自带的资源实现软件烧写,无需特别工具。