This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADC共模电压要求的疑问

Other Parts Discussed in Thread: ADS1248, THS4521

最近在做一个项目,项目中使用ADS1248做PT100的采样,电路是参考的数据手册中的电路,本来计划还有两路单端信号(0~5V,4~20ma)是通过单片机进行采样,后来考虑到单片机的ADC精度不高,而ADS1248这边又还有3路差分信号输入没有利用,所以准备使用1248来采样这两路单端信号。现在我有两个疑问,还请帮我解答一下。1、之前设计的是信号调理后用三个精密电阻分压,采中间一个电阻的电压作为差分信号,进ADC,但是发现共模电压不能满足芯片手册要求,如果要满足ADC要求,必须将单端信号处理成差分信号,不知道除了用差分驱动器等,还有没有别的简单一点的方法(我想到另外一种解决办法,不知道可行不,就是先将信号通过V-V转换为2~3V信号,再通过精密电阻分压,这样差模和共模信号都可以满足要求了)?2、在这个设计中,我考虑的采样方式是:先进行PT100的采样(外部820*2ma VREF=1.64V),再切换到内部VREF,轮换接通另外两路信号进行采样,这样做主要是为了另外两路采样不受PT100采样的影响(如果不接PT100,外部VREF就没有),我的疑问是这样是否可行,效率上怎么样?请知道的讲讲,先谢谢了!

  • 自己顶一下,有看到朋友没,出来说两句啊

  • 你按照datasheet 第86页的接法接就可以了。内部MUX切换速度很快,肯定不会影响。

  • 谢谢回复!不过我已经改方案了,用THS4521将单端信号变为差分信号,再进1248,仿真过,应该问题不大,只是增加了成本。不影响效率最好了。

    ps:如果按照datasheet的接法,应该在AINn接2.5V(5V供电的话),那么如果单端信号输入为0V时,AINp-AINn不是为-2.5V了吗,差分电压这么大,如果用内部VREF 2.048,哪怕GAIN=1,差分输入的电压也超过要求值了吧(±VREF/GAIN = ±2.048V),这样行不行哦,有点怀疑?