现在使用DAC7750IPWP做DAC转换,输出的4--20mA电流信号用于控制外部的阀门,现在有几个问题希望TI的工程师帮忙解答一下:
1、DAC7750IPWP的DVDD的供电电源为了确保其精度及芯片损耗,采用了外部的5V供电,但是我们使用的CPU是TI的TMS320F2808,它与DAC7750IPWP是通过SPI通讯的,那么TMS320F2808的SPI引脚是否兼容5V电平?为了防止芯片烧坏,我们飞线为3.3V供电,调试正常。但是另外一块板子用5V供电时也能正常工作,这是否说明TMS320F2808的SPI引脚可以兼容5V电平,或者说可以短时的运行?
2、DAC7750IPWP的输出Iout在使能输出4--20mA时,Iout是否可以长时间悬空,对芯片是否有影响?