This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1200EVM和ADS6444问题

您好:

        我们购买了TSW1200EVM评估板,和它配套的是ADS6444EVM板。现在使用中遇到了一些问题,请您帮忙解决一下。

        1、EEPROM Configuration Options有4的选项,但现在只能有一种选项好使;即按照PDF文档中说明设置J10和J11跳线,只能用一种状态,即J10的1、2脚联通,J11的1、2脚联通。设置成其他方式,软件提示不对。
        2、用评估板对信号发生器产生的信号采集,从软件上得到的数据和图形不对。使用A通道或B通道,采集信号为10MHz 正弦信号,幅值0.5vpp;用J12CLKIN通道输入采样信号,采样信号是用同一个信号发生器输出的,100MHz,正弦信号,幅值1vpp。从软件中得到的图形不是正弦信号。
        3、软件中的overlay "Unwrap Waveform"是什么意思?它与红色的图形区别?
       麻烦您给解答一下!谢谢!
  • 用评估板对信号发生器产生的信号采集,从软件上得到的数据和图形不对。使用A通道或B通道,采集信号为10MHz 正弦信号,幅值0.5vpp;用J12CLKIN通道输入采样信号,采样信号是用同一个信号发生器输出的,100MHz,正弦信号,幅值1vpp。从软件中得到的图形不是正弦信号。

    这应该是设置有问题, 采样率不够, 也许是采样时间或者滤波的影响