This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1232经常烧坏

Other Parts Discussed in Thread: ADS1232, ADS1230

电路图如附件所示,在使用中,ADS1232经常烧坏,这是为什么呢?

  • 1. 输入接固定直流电压,工作时用万用表量一下各管脚电压,看看是否在手册标注的范围内。

    2. 把R4,R5两个电阻拆掉,看看情况有没有好转。

    3. 从手册上看,晶振并没有通过电容接地。是否你买的晶振有电容接地的要求?不过就算接地,也应该接模拟地吧?

  • 建议:

    1.可以先与好的芯片做阻抗比对。

    2.用示波器需要确认一下AVDD,DVDD,模拟输入等Pin脚的电压是否有超出最大耐压。

  • 我在使用ADS1232的过程中也经常碰到过损坏现象,个人感觉如下:

    1. ADS1232的端口输入保护电路比较脆弱,一般都是从11,12脚或者22,23,24脚窜入的尖峰EMI或者浪涌脉冲造成其损坏,尤其以22,23,24居多。

    2. 建议R6,R7在1K左右,且前面加抗EMI器件,如果可能的话,建议对地和电源加钳位二极管

    3. 建议在22,23,24脚串入一个100~200欧姆电阻,对地加47P~100P电容,后面再加EMI器件。

    4.建议将芯片的模拟地,数字地,模拟电源,数字电源共用一个,将芯片周围划为模拟区,再统一单点连到CPU部分的电源和地上。(两者的地最好通过磁珠相连,而不是普通电感,切记!)

    5.布线的时候,尽量缩短CPU和22,23,24脚的连线

    6.有条件的话,将上述模拟区用屏蔽罩整个罩上。

    7.注意,ADS1232有一种慢慢损坏现象:比如转换结果慢慢漂移,或者结果突然变化很大,而检查前端输入无任何问题。

    8.继电器等容易产生火花干扰的设备一定要远离芯片。

    9.同样TI产的ADS1230似乎好些,可以尝试代换。分辨率20bit, 最小增益64倍,价格也便宜几乎一半!

  • 的确是这个问题,我正在调试,已经烧3次了,我的现象是不断电可以安全工作数日,断电后再通电就会损坏,搞不清是断电时损还是上电时损坏,损坏后数字部分工作正常,AD转换结果为0x800000或0x7FFFFF,不变化,我的数字通信线有47欧姆电阻,模拟输入为称重电桥,12V电瓶供电

  • 原来用ADS1210时对数字电源与模拟电源的上电顺序有要求,1232没见到有这样的要求,实践中是不是也有这方面问题呢?因为损坏的是模专部分,我先在模拟输入加ESD保护试试