Other Parts Discussed in Thread: DAC7718
请问:
PLC需要一个DA输出接口,提供0~10V的电压信号控制变频。感觉可以采用2种方式:
1) 利用一个DAC转换器,直接输出0~10V信号,再加一级跟随器;
2) 利用一个DAC转换器,输出0~5V信号,后跟一级运放进行2倍放大到0~10V,再加一级跟随器;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DAC7718
请问:
PLC需要一个DA输出接口,提供0~10V的电压信号控制变频。感觉可以采用2种方式:
1) 利用一个DAC转换器,直接输出0~10V信号,再加一级跟随器;
2) 利用一个DAC转换器,输出0~5V信号,后跟一级运放进行2倍放大到0~10V,再加一级跟随器;
你好,
你需要精度为多少位的DAC?告知我们可以帮助选型
Best regards,
Sulyn Zhang
Sulyn,
需要一颗12bit8通道DAC,10KHz转换频率即可。
最好是SPI接口,0~10V输出,最好可超压到11V(0~5V输出勉强也可,后加一级放大),相对精度1LSB。
谢谢!
你好,
根据你的需求,你可以看下这颗芯片,DAC7718。可以支持0~10V输出,供电范围灵活。
不过需要注意的是,如果你需要0~10V的”0V“,如过这个0V要非常精确比如要精确到几个mV,那么你需要双电源供电。如果”0v“的精度要求不高,你单电源供电就可以了,比如15V供电。
如果回答了你的问题,请帮忙点确认,谢谢!
Best regards,
Sulyn Zhang