Other Parts Discussed in Thread: ADS8422
在ADS8422手册P23页的figure34/35给出的电路中,在脚+VAREG与+VA之间接了一个0Ω的电阻,不知道其作用是什么?可以不接吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS8422
在ADS8422手册P23页的figure34/35给出的电路中,在脚+VAREG与+VA之间接了一个0Ω的电阻,不知道其作用是什么?可以不接吗?
+VAREG引脚的电压范围在3V-5V,+VA引脚的电压范围在4.75 V -5.25 V,如果两个引脚都使用5V供电,可以只接一端,焊接0欧姆电阻。如果+VAREG使用3.3V,则不焊接0欧姆电阻。
这里的0ohm电阻目的是为了实现单点连接,两个电压都接在5V,通过0ohm电阻连接防止由于两个由于电压差产生的回流。 就和AGND和DGND通过0ohm连接的道理是一样的。