.我现在使用的是sn65lvds93a芯片将16bit的LCD信号转化为lvds信号。我输入信号没有问题 但是用示波器测量芯片的时钟输出 电平好低呀 顶多0.5V。这个是什么情况/
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
.我现在使用的是sn65lvds93a芯片将16bit的LCD信号转化为lvds信号。我输入信号没有问题 但是用示波器测量芯片的时钟输出 电平好低呀 顶多0.5V。这个是什么情况/
首先先检查下引脚焊接情况,其次检查下硬件电路,电源电压是否正常,输入时钟是多少频率的?输出data有无信号?
电路图在之前的一个帖子我贴上去过了,芯片管脚焊接是没有问题,电压供应也是没有问题的。
那检查下上电时序,建议按照datasheet中的时序上电,保证PLL lock:
Power-up sequence (SN65LVDS93A SHTDN input initially low):
1. Ramp up LCD power (maybe 0.5 ms to 10 ms) but keep backlight turned off.
2. Wait for additional 0-200ms to ensure display noise won’t occur.
3. Enable video source output; start sending black video data.
4. Toggle LVDS83B shutdown to SHTDN = VIH.
5. Send >1 ms of black video data; this allows the LVDS83B to be phase locked, and the display to show black
data first.
6. Start sending true image data.
7. Enable backlight