Other Parts Discussed in Thread: AFE5801
AFE5801的内部参考电压是多少,手册上没有明确的说明啊。。。还有ADC转换的基准电压是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AFE5801
AFE5801的内部参考电压是多少,手册上没有明确的说明啊。。。还有ADC转换的基准电压是多少?
您好,AFE5801可提供内部或者外部参考电压选择。当选择使用内部参考电压时,数据手册第17页指出内部参考电压源通过一个Buffer提供1.6V 共模信号,ADC所使用基准参考电压也是这个。
如果您的问题已经得到解决,请在“这是否解答您的问题” 后,点击“是”按钮。 谢谢您的对TI的支持!
我和AFE5801的designer聊过了,这里的1.6V仅仅是共模信号,并不是内部参考。AFE5801的参考电压是1.4V,通过内部运放产生0.5V和1.5V给AD,所以AD的范围是1.5-0.5=1V。如果不是多片AFE5801,还是推荐采用内部参考电压。
你好,AFE5801支持两种数据模式,补码或者straight offset binary code,1.5V的code是fff只是举例,是straight offset binary code模式下offset为0时。
谢谢你的回答。还有两个问题:
1)datasheet第17页说VGA输出2Vpp摆幅的信号驱动ADC,为什么说AD的输出是0.5V~1.5V呢?按道理它是可以转换摆幅为2V的信号的。
The VGA/AAF can output 2Vpp differential swing without degradation in the specified linearity and can drive an
onboard 12bit ADC.
1)我如果选用DFS默认的格式(补码格式),那么输出的数字量和straight offset binary code模式下offset为0时输出的数字量一样吗?如果AD转换输出0.5V~1.5V的话,那么输出信号就应该时单级信号了。
谢谢!
您好,这里说ADC的输入范围0.5V~1.5V指的应该是单端的,也即可以达到1Vpp的电压幅度, ADC是差分输入时:Vppmax=2(0.5-(-0.5))=2Vpp 可能你会问,共模电压的问题,参见datasheet上面的输入端口原理图可以看出,内部有电容,是交流耦合的,所以不用担心这个问题。
你好。
1)这里的2Vpp是指AFE的输入是1.1到2.1,最大到2.1,这里面有1.6V的共模信号,经过转换,最后在内部AD上的是0.5到1.5.这里的drive并不是directly。
2)sulyn提到了,这里的0.5到1.5是单端,差分最大还是1。straight offset binary code相当于straight binary code 再减去offset。所以,补码不是offset为0的straight offset binary code