Other Parts Discussed in Thread: SN65HVD50
最近在使用SN65hvd50进行数据通信,发现这个片子在待机空闲的情况下温升有10℃以上,是在没有外接连线,没有任何匹配电阻的情况下,R和D测试均为低电平!如果在通信条件下温升有20多摄氏度。查找原因无果,换过不同批次的片子情况相同,麻烦大神给个指点!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65HVD50
最近在使用SN65hvd50进行数据通信,发现这个片子在待机空闲的情况下温升有10℃以上,是在没有外接连线,没有任何匹配电阻的情况下,R和D测试均为低电平!如果在通信条件下温升有20多摄氏度。查找原因无果,换过不同批次的片子情况相同,麻烦大神给个指点!!!
首先待机并不是不上电,待机也是有一定的功耗,只是器件处于低功耗状态,静态电流此时很低。
另外,R,D都是低电平, D是driver的输入端,R是receiver的输出端,要看下Driver的使能端DE以及receiver的使能端RE的配置,然后根据真值表判断输出状态。
除了温升,功能应用还正常吗?
低功耗状态都发热所以感觉不正常!
此款芯片没有DE,RE功能引脚。
功能都正常,就是温度有点高!
没有DE,RE的HVD50这款是没低功耗模式的,进入不了低功耗模式,一致处于enable状态。
或者根据热阻和输出功率计算下结温,跟实际测试的结温大致是否匹配。