Other Parts Discussed in Thread: TIDA-01469, TIPD149, ADS8881, TIPD115
采样速度达到1M以上,USB接口的。
非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
主要是用在岩石振动检测,想做成通用的采集板卡,±5V输入或±10V输入,1M采样率,通过USB输入到计算机中。
市场上有相关产品,但是想自己制作一下,所以寻求解决方案,请指教,谢谢
请问有相关产品链接可以参考吗?
通道数,分辨率是怎样的?
你好,
可以参考此链接的TI Design
http://www.ti.com/tool/TIDA-01469?keyMatch=vibration&tisearch=tidesigns
原理图:
http://www.ti.com/lit/df/tidrsk8/tidrsk8.pdf
这是无线传输的,要使用USB 传输,只需要将原理图中的无线模块替换成MSP430F55xx带USB接口的MCU 就可以实现了
那您看下这个方案:http://www.ti.com.cn/tool/cn/TIPD149
Hi Yaosong,
可以看一下采用ADS8881参考设计:针对最低失真和噪声的 18 位,1 每秒百万次采样 (MSPS) 数据采集块 (DAQ)
http://www.ti.com/tool/tipd115